Testing and Debugging the Project
During system validation it is essential that the KAS-IDE
"Integrated development environment"
An integrated development environment is a type of computer software that assists computer programmers in developing software.
IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger allows you to monitor the application program execution and to capture critical events and their data when they occur.
A Control Panel, designed with an internal editor, can be used to provide a basic interface.